Littelfuse Adds 3425L Series SMD Resettable PPTCs Series Created for High-Voltage Applications

3425L Series SMD Resettable PPTCs Series

CHICAGO, May 2, 2023 --  Littelfuse, Inc.(NASDAQ: LFUS), an industrial technology manufacturing company empowering a sustainable, connected, and safer world, announced the release of the 3425L Series SMD resettable PPTCs (Polymeric Positive Temperature Coefficient) overcurrent circuit protection devices.

The latest 3425L Series SMD PPTCs is an extension of the Littelfuse PolySwitch® family of resettable overcurrent protection devices, which provides resettable, high-voltage overcurrent protection in a compact, surface-mounted 8763 mm (3425 mils) size.

The new 3425L series is ideal for use in many applications, including:

  • Consumer electronics, such as power tools and televisions>/li>
  • Computing equipment and servers
  • Industrial robotics
  • Data center and telecom equipment

“Adding the 3425L Series to the PolySwitch product line delivers another clear performance advantage for electronics designers and their latest innovations,” said Stephen Li, a Global Product Manager at Littelfuse. “These new surface-mounted PPTC devices offer resettable high-voltage overcurrent protection, thereby reducing product warranty, service, and repair costs.”

The 3425L Series SMD PPTCs offer the following key benefits:

  • Resettable overcurrent protection with operational voltages ranging from 36 V to 60 V.
  • Compatible with high-volume electronics assembly, providing a compact 3.4 x 2.5 mils size surface mountable footprint.
  • Environmentally friendly with RoHS compliance and halogen-free manufacturing.

Availability

The 3425L Series SMD PPTCs are available in tape and reel format in quantities of 500 (3425L260/60) and 1,000 (3425L200/60 and 3425L300/36). Place sample requests through authorized Littelfuse distributors worldwide. For a listing of Littelfuse distributors, please visit Littelfuse.com.

For More Information

Additional information on the latest series release is available on the 3425L Series SMD PPTCs product page. For technical questions, please contact Stephen Li, Global Product Manager, sli2@littelfuse.com.

About Littelfuse

Littelfuse is a diversified, industrial technology manufacturing company empowering a sustainable, connected, and safer world. Across more than 20 countries, and with approximately 18,000 global associates, we partner with customers to design and deliver innovative, reliable solutions. Serving over 100,000 end customers, our products are found in a variety of industrial, transportation, and electronics end markets—everywhere, every day. Headquartered in Chicago, Illinois, United States, Littelfuse was founded in 1927. Learn more at Littelfuse.com.

LFUS-P

# # #

Back To Top